5/19/2019 12:15 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi The question is how many data do you want to export? Because, maybe you don´t need nothing, only with a few scripts and you can do the task. As you are running v6.0 you have the driver DDE, this meants you can create a connection with Excel and do the task. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/19/2019 1:22 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi You can connect the old archives to WinCC, then you can use the controls ActiveX Trends and Table Control to recover the data and export to excel. All this you can do it without extra add-ons. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/19/2019 1:32 PM | |
Joined: 12/8/2010 Last visit: 8/2/2022 Posts: 25 Rating: (2) |
Hi Could you explain more? Do you have any documentation to help me? How to I can export to excell? Best Regards |
5/19/2019 2:15 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi Sorry, my mistake!!! WinCC V6.0 don´t have the option to export to csv, then open with Excel. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on