5/19/2019 9:21 PM | |
Posts: 2 Rating: (0) |
Dear All, I have a problem with s7-200 cpu's. I did study manual and i cann't find the differences. I explain now, I have a system build up with a CPU224 with number 6ES7214-1AD23-0XB0 with a extension module EM223 (6ES7223-1BH22-0XA0) and a TD200. CPU is giving problems, i cann't connect the cpu from the computer anymore (MicroWin). So I cann't change software program and I cann't up- and download the software. I have a spare cpu224, 6ES7214-1AD21-0XB0. I thought to upload the software of above system into it. But I become errors. I did test this system connected to a TD200 and there are no problems. So, this spare unit and spare TD200 are oké. I haven't a spare EM223. I did study both manuals and i cann't discover the difference. Is there anybody who can tell me what's wrong. Thanks for the help. Louis van der Veer ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/20/2019 14:11:28New subject after splitting |
|
Follow us on