5/17/2019 3:20 AM | |
Joined: 6/24/2015 Last visit: 10/16/2023 Posts: 9 Rating: (0) |
Dear Sir, I want to install the software TIA V15.1 (Order No 6ES7822-1AA05-0YA5) install on the pc with OS Win10 1803 Enterprise , The user as Administrator role .First , I clicked the setup appliction , the everythings run good, and then asked the PC restart , and then ,I restarted the PC , and then , The PC shuted down , and started , and then PC run the application automaticly , and then the pc display the error message as follow: attachment 2019-05-16-003.jpg, and i clicked the <Show setup report > button , I got a text file as follow: I think the reason as highlight text . But I don't know how to handle them ? Thanks very much ! Xiaode 13:13:52 | BEGIN. Execution started. |
5/17/2019 10:13 AM | |
Joined: 7/9/2015 Last visit: 4/24/2024 Posts: 3812 Rating: (554)
|
Hi, do you have any virusscanner in use? If yes deactivate it and install again. Perhaps better deinstall all TIA components completely. How do you uninstall STEP 7 (TIA Portal) completely?Regards, Towome |
|
|
This contribution was helpful to2 thankful Users |
5/20/2019 2:08 AM | |
Joined: 6/24/2015 Last visit: 10/16/2023 Posts: 9 Rating: (0) |
Hi Towome, When I installing the TIA V15.1 , The computer running the defender , Is that means I should stop the defender ? Thank You ! Best Regards Jane Cheng |
This contribution was helpful to1 thankful Users |
Follow us on