5/16/2019 9:53 AM | |
Joined: 10/1/2018 Last visit: 8/23/2024 Posts: 74 Rating: (1) |
I have the same problem. The SF light of the PM module is ON and the BF light of ET200 is ON. TIA Portal says that the configuration data differs from the onlie data. I checked this and the configuration is the same. Could anybody help me with this? Find attached a picture of it. Thank you ------------------------------------------------------------------------------------------ AttachmentET200 error.pdf (280 Downloads) |
Last edited by: ismaelillo at: 05/27/2019 09:54:51Last edited by: Jen_Moderator at: 05/27/2019 14:24:29New subject after splitting |
|
5/16/2019 3:20 PM | |
Joined: 10/16/2007 Last visit: 9/11/2024 Posts: 629 Rating: (45) |
Hello, are you sure you have connected the power supply properly? Regards |
5/17/2019 9:34 AM | |
Joined: 10/1/2018 Last visit: 8/23/2024 Posts: 74 Rating: (1) |
I think so. Find attached picture. |
5/27/2019 4:55 PM | |
Joined: 10/1/2018 Last visit: 8/23/2024 Posts: 74 Rating: (1) |
I have it. You can see it in this attached picture. I really don't know what can be the problem. |
Follow us on