Industry Online Support
Technical Forum
10/7/2008 7:35 AM | |
Joined: 2/22/2008 Last visit: 2/2/2023 Posts: 39 Rating: (4) |
Hi All, Well an update, Pee Ell Sea's reply is indeed correct thanks!, so my mystery has been answer'd, but this issue is a regular on the Forum so I am wondering if between us we can come up with a convieniant solution! perhaps not involving some wires attached to Machine 24V or an external 24V Supply. I am thinking of a battery of some kind but i am wondering about the power requirement's of the adaptor? Any other ideas chip in! Thanks. Max |
10/13/2008 7:19 PM | |
Joined: 2/22/2008 Last visit: 2/2/2023 Posts: 39 Rating: (4) |
Hi All Another Update! I have spent sometime trying to answer this and think i have a solution im happy with. The USB PC Adaptor manual ( 6ES7972-0CA23-0XA0; 6ES7972-0CB20-0XA0) section 4.3 page 17, contains all the information regarding this. Siemens do infact sell a power supply (6ES7 972-0CA00-0XA0), however i have chosen to make one, all the required information is contained in the manual. Manual Attached. Regards, Max. i guess the moral of the question is to read the manual ! AttachmentPC_Adapter_USB_e.pdf (627 Downloads) |
Follow us on