5/23/2019 7:45 AM | |
Posts: 2 Rating: (0) |
Dear All, kindly suggest the upgraded version of speed controller ( SIEMENS MICROMASTER-VECTOR).These are obsolete and no more available. Appreciate your earliest response please. Best Regards, Ahsan Aziz
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/23/2019 09:39:47New subject after splitting |
|
6/3/2019 3:42 AM | |
Posts: 153 Rating: (7) |
Hello moneybhai That Depends on your old micro master, that it is with encoder or without encoder. If MM4 without encoder means go for G120 (any type-consider rating) If MM4 With encoder please select G120 with CU250. OR you can select S120 Drive for standard application. There are some migration tools available for MM4 to Sinamics, but it is not working now, may be some other tool is available, check that.
|
Follow us on