11/24/2014 8:14 AM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello Guybrows83, The sign regarding a positive or negative number is included while you convert INT to STRING with FC16(I_STRING) from IEC library. As an alternative, you can convert the input as INT to the BCD equivalent and then use HEX to ASCII conversion "FC95(HTA)" from TI-S7 converting blocks.In thiis case the positive sign has no meaning.A sample can be found here: https://www.automation.siemens.com/tf/WW/en/Posts/107469 The other strategy would be checking if possible to manipulate the output STRING before sending it to the printer. I hope this helps, Hamid Hosseini |
This contribution was helpful to2 thankful Users |
2/18/2019 9:58 AM | |
Posts: 1 Rating: (0) |
Thanks it works... |
This contribution was helpful to1 thankful Users |
5/23/2019 1:10 PM | |
Joined: 6/26/2017 Last visit: 4/3/2024 Posts: 4 Rating: (5) |
You can also use the VAL_STRG() to convert a numbers into strings. |
This contribution was helpful to1 thankful Users |
Follow us on