4/11/2012 8:52 AM | |
Posts: 19 Rating: (0) |
Hey Amit, after operator login, logout button must be enabled so thatoperator can logout i have attached the snapshot. |
4/12/2012 8:21 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Perhaps check User Administrator from WinCCExplorer? |
B r g d s , |
|
4/12/2012 10:54 AM | |
Posts: 19 Rating: (0) |
i have done with user adminstrator, but still logout button after login is disabled |
4/18/2012 8:35 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hello , Check the attachment to see how possible to define different short keys for log in and log out options. Check if this is the case.Also check the example here if it is compatible with your WINCC version? Track users' activities Best regards, Hamid Hosseini Attachmentuser.zip (145 Downloads) |
5/23/2019 9:01 PM | |
Posts: 4 Rating: (0) |
Here, thing is it is activating the logon screen only, thats why logoff was disabled. use a seperate button for log off and try once. |
Follow us on