5/24/2019 7:23 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi @shish, This is F-IOs of distributed safety---- All DOs are disabled until thay are successfully compiled in F program. (It should be used somewhere in Program). If this is done, then u can force or use VAT table to switch it ON. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on