5/25/2019 3:04 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello almohandiss; Your% MD40 parameter at the input of your Norm_X shows a value of 145.Actually, it should be a REAL value, 145.0. Notice how your MIN and mAX values are all in REAL (floating-point) format? See if Example 2 in this FAQ can provide hints: For an S7-1200/S7-1500 controller in STEP 7 (TIA Portal), how do you scale integer values in real numbers and vice versa for analog inputs and outputs? https://support.industry.siemens.com/cs/ww/en/view/39334504 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
5/25/2019 3:52 PM | |
Posts: 4 Rating: (0) |
is that true? |
5/27/2019 1:48 PM | |
Posts: 4 Rating: (0) |
The output is either 0 or 1 |
Follow us on