5/23/2019 12:19 AM | |
Joined: 12/7/2011 Last visit: 4/24/2024 Posts: 383 Rating: (9) |
Hi guys, I'am building a block icon and faceplate with WinCC 14. From the block icon, i've a C script to call the faceplate, and set a TagPrefix. Ths Script it's working fine, but an error appear in the Global Script Diagnostic Window. I would like to clear it, but i don't know the source of the error. Could anyone help me to understand the reasone? Thanks Regards. Duccio. AttachmentScript error.pdf (45 Downloads) |
5/27/2019 3:33 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1641)
|
Hello Duccio If you send us the Script we can see or guess whats wrong. You can also use printf to do diagnostic poutputs to see where exactly in which line the error occurs: http://support.automation.siemens.com/WW/view/en/22196775 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on