5/29/2019 9:14 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hello dchartier, Sorry for continuing your old post, You have said right, SFC20 BLKMVE is a right to block to use, But, How to mention the SRCBLK, DSTBLK information, Bcoz, In PCS7 Blocks having only "Connect to address" or "Textual interconnection" way of interconnections, I unable to use connect to address. How to I can represent the SRC address detail? ------------------------------------------------------------------------------------------ |
Last edited by: Maruthakasi_S at: 05/30/2019 11:22:34Last edited by: Jen_Moderator at: 05/31/2019 06:55:13New subject after splitting Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
5/29/2019 10:40 PM | |
Joined: 9/27/2006 Last visit: 4/22/2024 Posts: 12257 Rating: (2665)
|
Hello Kasi SP; You will have to build up the ANY pointer before you use it as a parameter in the BLKMOV, as shown in the following document: https://support.industry.siemens.com/cs/us/en/view/674578 Hope this helps, |
This contribution was helpful to1 thankful Users |
5/30/2019 12:09 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi 93Mustang, You can create separate FC (probably in STL) for volume data move with input parameters in integers datatype. (e.g. source_start_byte_no, desti_start_byte _no, no_of_bytes etc). Then u can call this block to CFC chart.
|
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
Follow us on