5/31/2019 11:31 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Yes, you can implement an OPC UA Server on the IOT2000 and yes you will have to implement it yourself as the only image we provide is an example image with a few software tools. You can check out this application example as a reference on an OPC UA Server, although I would recommend using C++ or python due to stability issues with nodejs. If you need the IOT to act as an OPC UA Client on the other hand, node-red provides a handy solution. There are two physical I/Os on the IOT that support interrupts. The Pin layout is the same as on the Arduino Uno and you can use the mraa library to configure them. Kind regards! |
This contribution was helpful to1 thankful Users |
Follow us on