6/2/2019 6:32 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Just an idea that may or may not work and as always I'm fooling around to find out what may work. Attached is a project created in TIA13-SP2 with only a panel in it of the version you wanted. And here's a link for the above project upgraded to TIA15-1 update1 containing the v13.0.1.0 and the CPU you mentioned in your first post. See if you can use either to copy your existing work to them and please let us know if that works for you. Attachmentwincc13_.zip (90 Downloads) |
6/3/2019 6:42 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
KaI.A, thank you for you help. Unfortunately I have TIA15 so I cannot open TIA15-1 project (( But of course I have checked the same - converted my old V13 project into V15. Unfortunately, in the converted project WinCC RT is not recognized as 13.0.1.0 but is recognized as 15.0.0.0. I think it's due to abscence of WinCC RT 13.0.1.0 in the HW catalog. So, the Q, which still no one can give an idea - can I install WinCC RT 13.0.1.0 into HW catalog of TIA V15 and how? |
Follow us on