6/4/2019 11:03 AM | |
Posts: 1 Rating: (0) |
Hi, The same issue for me. Installed software: I have installed TIA Portal V15 a) Simatic step7 Basic/Professional V15 b) Simatic Wincc Basic/ Comfort/Advance V15 c) Simatic Step 7 PLCSIM V15 Project Details: a) CPU 1214 b) HMI - KTP 900 Basic both are integrated in same project. Simulation: a) PLC - I have run the PLC V15 and download the PLC project. Well going to run and can monitor. b) For HMI - When i compile and start the simulation of HMI by using the "Start simulation" button just below help button on the top navigation bar. Result: SIMATIC HMI BASIC RUN TIME SIMULATOR HAS STOPPED WORKING. I am using Wincc RT Advance, RT Professional and Wincc Professional License with V15. I am not sure is there any licence Wincc RT Basic need to use? and this is the reason it stopping the simulator. Please advise. Very very urgent. Thanks, JP [snip] ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/04/2019 14:13:24New subject after splitting Last edited by: Jen_Moderator at: 06/04/2019 14:14:28Removed phone-number. |
|
Follow us on