5/28/2019 10:07 PM | |
Joined: 1/3/2019 Last visit: 12/16/2022 Posts: 64 Rating: (0) |
Hello friends.. I make a project with Wincc Explorer 7.4v , my windows is 7 64bit , I want to copy my project from my laptop to my pc.. Two windows are same, and two wincc are same... i read wincc copy forums.. they tell use wincc dublicator but i dont understand what do i should to do.. Can you help me please...thanks... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/29/2019 11:26:21New subject after splitting En. M.ABZADEH |
|
5/29/2019 11:36 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Hi Stop WinCC Runtime, and close WinCC. Copy and paste the full directory of your project. After you copy the project to the new PC, you will have to change the name of the server, you will se the warning. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
6/7/2019 6:18 AM | |
Joined: 1/3/2019 Last visit: 12/16/2022 Posts: 64 Rating: (0) |
Thank you... |
En. M.ABZADEH |
|
Follow us on