1/29/2017 8:44 AM | |
Posts: 4 Rating: (1) |
"Commissioning Sinumerik 828D and HLA Module with Third Party Analog Drive (Bosch Analog Drive) " Dear Sir, We have commissioned Sinumerik 828D Basic and HLA Module with Third Party Analog Drive but we have been facing following problems. 1. We are not able to find Startup file for Milling Package. 2. There is no particular .SDB file for HLA Module as like ADI4.sdb card. 3. Unable to find exact Analog setpoints in HLA Drive Module. We have commissioned MCP, PP and HLA module drive is also commissioned but unable to do "Axis Assignment".When we try to configure HLA module without Hydraulic parameters it shows that Reading Data. it will go to infinite mode. Even after entering default values in hydraulic parameters also we do not get analog voltage at Analog points. We request you to provide following files. 1. Startup file for milling and turning package. 2. we are using two HLA module for 3+1 so do provide .sdb file for HLA Module according to our requirement. 3. Commissioning manual of Sinumerik 828D and HLA Module. 4. Parametes manual. It will be great thank full to you. Regards Venkatesh Nayak ------------------------------------------------------------------------------------------ |
Last edited by: Venkatesh Nayak at: 1/29/2017 8:47:00 AMLast edited by: Min_Moderator at: 1/30/2017 4:26:12 PMNew subject after splitting |
|
1/29/2017 9:12 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please follow this link where you will find commissioning, service, component manuals of 828 system. For your files I would suggest you to contact your nearest Siemens RSC office. HTH. |
This contribution was helpful to1 thankful Users |
5/29/2017 3:15 AM | |
Joined: 9/15/2016 Last visit: 4/19/2024 Posts: 6 Rating: (0) |
I am also commissioning Similar Application. I have loaded standard SDB and IB file. I am able to read the actual of encoder. Does any one have idea on how to make HLA healthy. Analog set point for drive is not coming. If any one can share experience it will be great help.
|
Follow us on