3/23/2018 4:24 AM | |
Posts: 2 Rating: (0) |
Hi Banconi, |
Last edited by: MinhPhong at: 3/23/2018 4:29:11 AM |
|
This contribution was helpful to1 thankful Users |
3/26/2018 1:02 PM | |
Joined: 8/3/2009 Last visit: 5/8/2024 Posts: 12909 Rating: (1645)
|
Hello banconi you also have to open the Ports that are needed for loading the HMI Panel. The used ports you can find at: https://support.industry.siemens.com/cs/de/en/view/109742297/87204625803 (you have to scroll down) --> And you should use Ethernet insted of PN_IE on Panel Transfer Settings and in TIA Portal Transfer Settings because the PN_IE works only with MAC Adress broadcast packages and this wont work with VPN connection. -> in newer TIA Versions you can also use PN_IE by selecting "Show devices with the same Adress" Bye Murof |
Last edited by: Murof at: 3/26/2018 1:04:55 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to4 thankful Users |
5/28/2021 8:53 AM | |
Posts: 2 Rating: (0) |
Thanks very much, I enabled all the ports named "HMI load" and it worked for me.
|
Follow us on