6/14/2019 8:01 AM | |
Joined: 11/7/2017 Last visit: 10/22/2023 Posts: 30 Rating: (1) |
Dear experts, I have 2 server and 2 clients configuration. I am facing some strange problem in my wincc. i am not able to see the connections of server 2 in clients,resulting my redundancy of server is not working. same case connections of clients seen only from server1,not in server 2. many times i generated server data and downloaded ,no use all clients and servers pinging each other ,i have checked the network connection. I am not getting redundant partner in server data in configure(Pic attached) Please suggest me the solution....... Attachmentserver_issue.zip (32 Downloads) |
6/14/2019 8:14 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32893 Rating: (4066) |
Is this the same problem as in this topic? |
6/14/2019 8:46 AM | |
Joined: 11/7/2017 Last visit: 10/22/2023 Posts: 30 Rating: (1) |
yes the same problem.... |
6/14/2019 9:28 AM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 951 Rating: (13) |
Closed, because the question was posted twice: Server package file issue The Helping Hand |
My Forum is the place to personalize your profile, |
|
Follow us on