12/23/2016 2:00 PM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Hi yasinEncoder, This should be possible.. When you run the setup and the system shows the "Installation type" screen (which is the screen after the screen where you can set the user information), you must activate: "Package installation" select the package and then it must be possible to click on "Browse" to set a different installation path. |
If I could help you, you can use the RATE button. Thank you. |
|
12/23/2016 3:09 PM | |
Posts: 57 Rating: (1) |
Hello dear Oreca I just did what you said but there isn't any "Brows" key. please see the attached picture. |
12/23/2016 4:03 PM | |
Posts: 57 Rating: (1) |
I already did it but I couldn't change the installation path Originality, there isn't any "Brows" key. |
Last edited by: yasinEncoder at: 12/23/2016 4:04:53 PM |
|
Follow us on