6/16/2019 1:30 PM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
hello Does 6SE6400-0PM00-0AA0 AOP or BOP ? Where can used in backup download/upload ? |
6/16/2019 4:13 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Sherief; The part number you show is for a door-mount support for either a BOP or AOP on a MM4 drive. If you purchase it you can install either one and access it on your cabinet door. With an AOP you can upload and download MM4 parameter sets: https://support.industry.siemens.com/cs/us/en/view/9945850 Hope this helps, |
6/18/2019 9:53 AM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
Thanks for reply... please advice optional card used to connect my USB/RS232 cable to the drive for backup |
6/18/2019 10:25 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please check below link. MICROMASTER 4: Uploading and downloading drive parameters using STARTER MICROMASTER 4 (MM4), SINAMICS G110 / G120 (CU 2x0x): RS232 / USB Adapter MICROMASTER 4 (MM4): Using DriveMonitor after an AOP |
Last edited by: Jen_Moderator at: 06/18/2019 13:46:25Optimized links. |
|
6/18/2019 11:15 AM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
Thanks for this helpful links... but in my Micromaster I can not see 9 bin standard RS232 socket |
6/18/2019 11:26 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
In first post you mentioned about 6SE6400-0PM00-0AA0 kit. You can use it. For more detail information check/refer MICROMASTER 4 (MM4): Serial interface ports FAQ. |
Last edited by: Jen_Moderator at: 06/18/2019 13:47:01Optimized link. |
|
6/18/2019 12:16 PM | |
Joined: 10/14/2009 Last visit: 10/17/2022 Posts: 140 Rating: (1) |
Thanks for your replies What I need to take backup from the drive. so I asked if I can use 6SE6400-0PM00-0AA0 ? or use serial communication and drive monitor |
Last edited by: sherief at: 06/18/2019 12:24:11 |
|
6/18/2019 12:48 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Part or MLFB number 6SE6400-0PM00-0AA0 which you mentioned is for kit which is useful to mount BOP or AOP on operater panel. Please refer your MM4 connection termination & settings. You can connect the appropriate adapter & upload/download parameters. For more information refer attached sheet. HTH. |
This contribution was helpful to1 thankful Users |
Follow us on