6/17/2019 10:01 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi OilGasOffshore, where did you get this information?
In the compatibility tool for PCS 7 V9.0 you can find the information that PCS 7 V9.0 SP1 and PCS 7 V9.0 SP2 is tested and released for Window 7 and Windows 10. All software that is listed with a green mark is also tested and released from Siemens on all operation systems (expect if there is a footnotes). So you can use Windows 10, PCS 7 V9.0 SP2 and SIMATIC NET SOFTNET-IE RNA V14 on the same PC. With regards |
This contribution was helpful to1 thankful Users |
Follow us on