10/25/2017 10:39 AM | |
Posts: 146 Rating: (7) |
Can anyone help? Milos |
10/25/2017 11:57 AM | |
Posts: 531 Rating: (34) |
http://www.makeuseof.com/tag/windows-10-slow-boot-issues/ or could be maleware or anything else taking to long. Network is up and working fine? |
10/25/2017 12:49 PM | |
Posts: 146 Rating: (7) |
It is brand new PC, it was not connected to internet so I believe that it does not have malware. Network is working fine. I noticed it on two applications, both with Windows 10 and WinCC clients. I just want to know what is the condition for WinCC autostart process to start activationg application, is there maybe delay for this start in windows... |
Follow us on