6/19/2019 8:55 PM | |
Posts: 16 Rating: (0) |
To add I have also change the names of the AS. They do not follow the standard AS01.... That could influence the XWP devices import? ...sent from App |
6/27/2019 5:54 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (6) |
Can anyone help me on this question, since the reply from Siemens is taking quite some time. Thanks, Bruno |
Thanks, |
|
7/1/2019 12:00 PM | ||||||||||
Joined: 7/25/2012 Last visit: 4/25/2024 Posts: 241 Rating: (68) |
Hi Bruno, I'll recommend to you to go on the extranet (in case you are from VAP) or on BT Academy site (in case you are internal Siemens employee) and see the online training (e-learning) with the name:
There should be most of answers on your questions. My sugestion is that you have probably missing or wrong installed a part of XWP and that why your installation doesn't work correctly. Please, try to reinstall you XWP + ABT libraries, especially ABT Graphics library for Control Point. I'll suggest, that may be wrong configuration for your installation of ABT Site. There is special files "Feature configuration" which must be configured from a country tool manager. Ask local Siemens support for that.
|
|||||||||
Best regards, |
||||||||||
This contribution was helpful to1 thankful Users |
Follow us on