6/14/2019 1:34 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Please refer attached sheet. Will help you to set spindle related data & interfacing signals. HTH. Attachment828 spindle MD & interfacing signal.pdf (53 Downloads) |
6/14/2019 1:49 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
31020 [0] - for motor encoder. 31020 [1] - is for external encoder. Set 31020 [1] = 1024. & check. |
6/17/2019 12:27 PM | |
Joined: 5/20/2016 Last visit: 7/7/2023 Posts: 32 Rating: (0) |
I have read in this thread : https://support.industry.siemens.com/tf/WW/en/posts/840d-with-611d/91178?page=0&pageSize=10 that encoder 1 is for Motor and encoder 2 is for external measuring. So i changed all setting for encoder 2 : 30200 $MA_NUM_ENCS[AX3]=2 30220 $MA_ENC_MODULE_NR[0,AX3]=1 30220 $MA_ENC_MODULE_NR[1,AX3]=1 30230 $MA_ENC_INPUT_NR[0,AX3]=1 30230 $MA_ENC_INPUT_NR[1,AX3]=1 30240 $MA_ENC_TYPE[0,AX3]=0 30240 $MA_ENC_TYPE[1,AX3]=1 30242 $MA_ENC_IS_INDEPENDENT[0,AX3]=0 30242 $MA_ENC_IS_INDEPENDENT[1,AX3]=1 Also P1192(0) is [2] Encoder2 now in Axis diag, i can see that "Measuring system 2 Active" is enabled , and when with hand turning spindle ,encoder start to counter .and MD30250[1] ACT_POS_ABS start to counter . but error is same. any person have another idea ?
|
6/18/2019 11:00 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, Please refer SINUMERIK 828D commissioning CNC manul, chapter 5, & for commissioning spindle refer page 97. HTH |
Last edited by: Jen_Moderator at: 06/18/2019 12:38:00Optimized link. |
|
6/18/2019 3:12 PM | |
Joined: 5/20/2016 Last visit: 7/7/2023 Posts: 32 Rating: (0) |
i checked all machine data and parameters , all things is ok i done 10 times commissioning, but until now ,Spindle with encoder( P1300=21 ) dont working . |
Follow us on