6/18/2019 3:56 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1734)
|
Hello Which TIA Portal Version do you use exactly? -> which Button can you press on the Panel? -< is already a Programm loaded on the Panel? - Load a Project with a Button and use the Systemfunction here to StopRuntime. What happens then, are you able to see the settings then? The Basic PAnels usually have no buffered internal Time. So you should make a Time synchronisation wiht the PLC which has a remanent clock: https://support.industry.siemens.com/cs/ww/en/view/69864408 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on