6/18/2019 8:45 AM | |
Joined: 6/18/2019 Last visit: 4/3/2024 Posts: 9 Rating: (0) |
Hello! I updated the project from TIA b13 to TIA b14. Plc 315-2pn / dp. When starting the simulation, everything is fine, but as soon as I connect to the simulator online, the CPU gives an error. I put the cpu into stop mode and back to run, everything is fine, but as soon as I want to go to the function block or re-enter the main page of the cpu program, I get an error. Photos with an error attached. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/18/2019 10:53:22New subject after splitting |
|
6/19/2019 12:36 AM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2348)
|
The posted image tells you what is going on. The online and offline configuration are very different part #'s. In the diagnostics status window, it tells you what the online and offline part #'s are. Figure out which is correct and fix the other one.
|
science guy |
|
Follow us on