6/20/2019 6:43 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Salutations, I have attached a program with a product counter,what I was looking to achieve was to use a secondary counter to count down from 30000 and then reset itself with a flag once target is achieved. I have managed to do this but there is a reset for a incremental counter but I dont want this to reset the count down until it has reached its target which at the moment it is doing.I still require the reset for the incremental. you will see more clearly from the simulation of the program.I hope you can provide some guidance. thank you for your patience Ade AttachmentACM_DATA_V2.zip (176 Downloads) |
6/20/2019 7:36 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
unfortunately only the b030 counter works...see attached jpeg |
6/20/2019 7:45 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
If you make it so as I wrote then you became the correct function. AttachmentCount down.zip (163 Downloads) |
6/20/2019 7:51 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Winner winner....Thank you for your patience |
This contribution was helpful to1 thankful Users |
Follow us on