7/12/2017 3:55 PM | |
Joined: 4/11/2014 Last visit: 9/13/2021 Posts: 22 Rating: (0) |
Hi Everyone, I am using TP1200 for my project with S7416H system(with CP443) and IM153-4HF. Software part i am using step7 5.5 sp4, wincc 7.3 and for Touch Panel TIA V14. In this project i am using Ring topology to communicate with IM and CPU 416H in integrated PN of the CPU. I am now wondering is it possible to add the TP1200 in Ring network by adding GSD files in my HW configuration? The problem is now i cannot find any GSD file for TP1200. Otherwise its easier to communicate the TP1200 with CP443 of 416H system right... But if i could be able to get the GSD file for TP1200 its easier to add in the Ring network. Can anyone please tell me a solution for the Touch panel or it is wise to add the communication using CP443. Please see my attached System configuration. Thanks.... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/13/2017 10:48:59 AMNew subject after splitting |
|
7/28/2017 2:20 PM | |
Posts: 50 Rating: (3) |
Hi, Can you please share the MLFB numbers of TP1200 HMI??? |
6/22/2019 6:41 AM | |
Joined: 11/9/2008 Last visit: 5/7/2024 Posts: 402 Rating: (6) |
Hi, I have same application. Have you able to add TP1200 in Ring Network? Please let me know. Regards, Yogendra |
Follow us on