6/21/2019 9:33 AM | |
Posts: 2 Rating: (0) |
Dear Thunderstorm , We have PCS7 V7.1 and would like to upgrade it to V9 . This would include
What are the licenses that will be affected? Attached excel sheet all licenses that we have Thanks in advance
------------------------------------------------------------------------------------------ AttachmentSIEMENS PCS7 license.xlsx (516 Downloads) |
Last edited by: Jen_Moderator at: 06/21/2019 13:24:07New subject after splitting |
|
6/24/2019 9:52 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Mr_Simo, the needed licences for the architectures can be found in the manual SIMATIC PCS 7 Standard Architectures (V9.0). And the licences can be upgrade with Update/Upgrade Packages. With regards |
6/24/2019 10:27 PM | |
Posts: 2 Rating: (0) |
Thanks Dear Heisenberg. I tried the upgrade link you posted before . However the packages are really confusing , for example 6ES7652-3AC17-2YA0 , I can't find equivalent to it in the upgrade packages. Also 6ES7833-1CC02-0YA5 , can't find an upgrade package to it , however I can find 6ES7833-1CC26-0YE5 as a new version. Third is 6ES7653-2BA00-0XB5 , I can see it's still active , when I do the upgrade will it still be valid? can you please help with these two specific licenses? Thanks in advance for your support. |
6/25/2019 11:09 AM | |
Joined: 11/22/2016 Last visit: 1/19/2024 Posts: 35 Rating: (3) |
Mr_Simo, For upgrade6ES7652-3AC17-2YA0, you need to buy 1x6ES7652-8AX28-0YE0 (7.1->8.2) and 2x6ES7652-5AX58-0YE0 (8.2->9.0), because 6ES7652-3AC17-2YA0is for two OS Station. License 6ES7833-1CC26-0YE5 is upgrade of F-system 6.x to 6.2. OS RT PO is unchaged during upgrade for OS station. More info you can find in Catalog STPCS7 https://support.industry.siemens.com/cs/document/109745632/catalog-st-pcs-7-(system-components)-simatic-pcs-7-for-v9-0?lc=en-ww |
This contribution was helpful to2 thankful Users |
Follow us on