6/25/2019 11:45 AM | |
Joined: 9/20/2017 Last visit: 3/20/2024 Posts: 27 Rating: (0) |
hello everyone i am using IM 155-6PN HF, I want to generate an alarm when IM fault generate. i have one program which is attached below. but it is not working properly. if i am power off the im then also the final IM FAULT bit is countinuous zero. can anyone suggest me more ? ------------------------------------------------------------------------------------------ AttachmentOB70.pdf (42 Downloads) |
Last edited by: The Helping Hand at: 06/25/2019 14:19:09New subject after splitting |
|
Follow us on