6/17/2019 8:53 AM | |
Posts: 2 Rating: (0) |
hi i am getting almost same error on PCS7 v8.2 . Initially all drivers were visible but the moment i installed plcsim on pcs7 started working slow as well as not able any drivers visible. i am using: windows 7 enterprises sp1 -64 bit ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/17/2019 10:37:02New subject after splitting |
|
6/26/2019 9:04 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi Talwar, Did you try the solution from the STEP 7 Conference?
Another solution you can find here with the s7oiehsx.exe in the attachment.
Another solution is to open the path "C:ProgramData\Siemens\Automation\SIMATIC OAM\data\LogDivices" and copy the XML files from the working installation to this folder. If after a PC restart the XML files are gone, only a complete reinstallation helps. With regards |
Follow us on