6/26/2019 9:39 AM | |
Joined: 9/2/2013 Last visit: 9/19/2024 Posts: 128 Rating: (0) |
Hi, Got some issue with our redundant servers and hopefully guys you can assist me on resolving this. We have two servers that are fully redundant, Server A is the master and Server B is standby. I have downloaded the entire project to Server B, And everything was completed. When Server B is synchronizing with Server A, the connection of our client was interrupted for some unknown reason. Therefore , I am force to re-start server A hoping that the redundancy will work and all client station will switch to Server B. Everything went fine and working. When server A restarted. I downloaded the entire project to Server A and started the runtime. Again, everything went fine. My problem now is that I want to put server A to master since this is our original configuration of the system. Unfortunately when I am trying to deactivate Server B runtime I got a pop-up message as follows: "The partner server cannot assume the function of the local server. If you disable the local server, this redundant operator control and monitoring server system will no longer be available. Do you want to continue?" This is the first time I seen this pop-up message and I'm worried if I continue with this our client will loose connection again with the server. Kindly help me please in solving this issue. I''ve check the status of redundancy for both server and I enclosed herewith as an attachment. Kind regards, AttachmentAttchment.zip (335 Downloads) |
6/26/2019 2:38 PM | |
Joined: 9/2/2013 Last visit: 9/19/2024 Posts: 128 Rating: (0) |
Hi, Can you let me know which diagnose log file I have to check regarding with redundancy? REgards, |
6/27/2019 4:33 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear PCS 7, Let me give some inputs as well, It seems like the OS A and OS B are conflicting with each other. Can you also check the below items? 1. The Time Synchronization between both station, make sure they are synchronized. 2. The Netpro connection name, make sure they are the same. 3. The ethernet (terminal bus) and serial link (redundancy link) are connected without issue. 4. The redundancy setting is configured correctly, (Sync through Serial COM port) 5. The Simatic Shell redundancy is configured correctly. 6. The user right is okay, able to access each other station and folders without the need to key in a password. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
6/27/2019 7:38 AM | |
Joined: 9/2/2013 Last visit: 9/19/2024 Posts: 128 Rating: (0) |
Hi, I'm try checking winCC_sys_02 of both servers, honestly I don't know what to look for. I attached herewith the diagnostic logs for both servers and hope you can help in interpreting the logs. REgards, AttachmentDIagnostic_logs.zip (219 Downloads) |
6/27/2019 12:23 PM | |
Joined: 9/2/2013 Last visit: 9/19/2024 Posts: 128 Rating: (0) |
Hi George, Thank for all your support. I have atttached herewith the SIMATIC_S7_Protocol_Suite_01 log for Server A. I notice the message "Redundancy error: Connection "RTU_AS" is not redundant!" . Can you help me how can I rectify this error. We have 2 PLC AS1 and RTU_AS. It seems that the connection on RTU_AS is not redundant. REgards, AttachmentProtocol Suit.zip (224 Downloads) |
Follow us on