2/16/2018 3:31 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hey, did you prove your display Settings of your Engineering System,? Follow this FAQ https://support.industry.siemens.com/cs/ww/en/view/90301561 With best regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
This contribution was helpful to1 thankful Users |
2/16/2018 9:06 PM | |
Posts: 8 Rating: (0) |
Excellent point, but this is for Mobile Panel 277F IWLAN. I'm getting the hardware soon and will be able to check it |
7/1/2019 10:33 AM | |
Posts: 45 Rating: (0) |
Hi Cumulus, I checked your link, but that is for Win7 and/or Win8. When I try to change the settings in Win10, it didn't solve my problem. My project is converted the long way: OP17 in Protool > OP177B in WinCCflex > OP177B in TIAv13 > TP1500 in TIAv13 > TP1500 in TIAv15.1. Text from the display is finaly converted to "WinCC_Flexible, 43px", a size which is not available in TIAv15.1. Even changing them to an existing size of 48px didn't solve the behaviour. The Text looks like to be shown bigger in the simulation-modus. The real TP is not available at the moment, so I can't test the real life. In the attachment some of the screens, both in design as well as in simulation. Any idea how to solve it?
AttachmentTP1500_DesignAndSimulate.zip (60 Downloads) |
7/1/2019 11:17 AM | |
Joined: 7/5/2013 Last visit: 9/24/2024 Posts: 3112 Rating: (512) |
Hello wideko, have a look here: Why are fonts and objects shown shifted on a PC Runtime system or operator panel? Looking at your screenshots it seems, it is not only about the font size. E.g. in 001_BasisScherm_48 the text "KEUZE:" is in another position compared to the objects above. Do you use several languages where the text field for the language used in simulation starts with a line break? If you use only one language, did you already "rebuild all"? Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to1 thankful Users |
Follow us on