7/1/2019 9:44 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Salimim6, Do you use PCS 7 V9.0 oder PCS 7 V9.0 SP1? Because PCS 7 V9.0 is not tested and released with CEMAT V9.0 SP1. So, if you use not released Software and run into problems, Siemens will not able to help you. The message "Connection to S7$Program(2) could not established" is shown, when there is no communication between the AS und WinCC Runtime, this can have many reasons:
With regards |
This contribution was helpful to1 thankful Users |
7/1/2019 11:57 AM | |
Posts: 3 Rating: (0) |
Hi thanks for your answer. I never checked that file before and I'm unable to understand what the recorded events are. Best regards |
Follow us on