7/2/2019 8:06 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Hi michigna, with UAExpert it is possible to use monitoring (polling) and subscrition mode. Which one do you use? The settings regarding the publishing intervals shouldn't matter when using monitoring mode. But which update cycle do you want to achieve? Update cycles faster than 1s or 500ms are VERY fast in WinCC systems, so reading data faster than that doesn't make sense. If you need to record "high speed" data from a PLC there are better ways than reading it via WinCC. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on