7/3/2019 10:02 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see attached screenshots. I have a meter-counter that is unintentionally reset when the machine is switched off and on again. To fix this I want to use a FB with STAT variables instead of the FC with TEMP variables for the meter counter logic. I have made the FB and checked that it is only used in OB1. When I open OB1 and try to replace FC12 with FB12 the system tells me it is an "invalid statement" Why is that an "invalid statement" and what is the correct way to do this? AttachmentFB12.zip (27 Downloads) |
Follow us on