5/16/2019 9:18 PM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2667) |
Hello rogerdc; The 7SJ82 relay is part of the Siprotec 5 family, programmed with DIGSI 5: You should find all the information you need you need in chapter 3 of the following manual: DIGSI 5 Engineering Guide – Manual https://support.industry.siemens.com/cs/ww/en/view/109742329 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 05/16/2019 21:18:36Last edited by: dchartier at: 05/16/2019 21:36:13 |
|
This contribution was helpful to1 thankful Users |
5/17/2019 8:55 PM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2667) |
Hello rogerdc; The Engineering manual suggested earlier contains information on IEC 61850 compatibility for Siprotec 5/DIGSI 5 relays, as you can see tin the attachment below.So you only need to configure the relay's Ethernet port through DIGSI 5 to access IEC 61850 functionnalities. For more information on IEC 61850 reporting available on your relay, open the following manual: SIPROTEC 5 PIXIT, PICS, TICS IEC 61850 – Manual https://support.industry.siemens.com/cs/ww/en/view/109742445 |
7/3/2019 8:53 AM | |
Joined: 10/9/2007 Last visit: 5/13/2024 Posts: 1241 Rating: (115)
|
Hi Contact Power Academy in Colombia. They are responsible for the region. Perhaps they can offer a special training on your office. ColombiaPower Academy CO Siemens S.A. |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on