7/4/2019 8:49 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (68) |
Hello ColinMai, could you give us more information about your system, like discribed here: could you also decribe your problem a little bit more precisely? Giving more information will help the forum community to help you with your problem :) Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
7/4/2019 1:06 PM | |
Joined: 7/5/2013 Last visit: 4/25/2024 Posts: 3075 Rating: (505) |
Hello ColinMai,
do you have the same problem, when loading the application to a panel? Is the full text shown in "design" mode (where you create the screen resp template)? If second answer is yes, have a look in this FAQ. If it is no, then either make the text field bigger or use a line break or use a smaller font. Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to1 thankful Users |
7/5/2019 5:49 AM | |
Joined: 9/1/2018 Last visit: 7/14/2022 Posts: 39 Rating: (3) |
Thank you very much based on your support, I finally can solve my problem. |
Follow us on