8/21/2018 7:30 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi shoot_nick, First: Never create your own tags in WinCC by linking them to instance DB's. It's not what PCS7 is about and during a full compile of the CFC program, the whole DB/FB/FC blocks are rearranged so that does not work. You have setup the s7_m_c attribute for the tag so that is good. Did you also set s7_m_c for the block itself? You have to allow the block to have the operator and control property as well. If it still does not work, you can upload (or share through PM) your code, so I can take a look.
|
If I could help you, you can use the RATE button. Thank you. |
|
8/21/2018 9:49 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
I think Harry forgot the ' at the end --> S7_xm_c :='Value,true;'
|
Last edited by: Oreca at: 8/21/2018 9:50:38 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on