7/9/2019 6:32 AM | |
Joined: 4/3/2012 Last visit: 4/24/2024 Posts: 18 Rating: (1) |
In parameter 595 I can change the Technological unit selection for the PID. If I change p595 to 20 then the graphic for the PID shows psi. But if I try to enter 50.0 for my setpoint it says it is out of range. Where do I change the max limit (max scale value) for the Analog and Setpoint. And how do I scale the analog input to the actual? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/09/2019 07:30:11New subject after splitting |
|
Follow us on