7/11/2019 7:53 AM | |
Joined: 10/18/2006 Last visit: 2/9/2024 Posts: 120 Rating: (15) |
Hi harclerode, in my past I had this error when the enginieering data was not consistent resp. not up to date on PLC and HMI. So you wrote you already redownloaded the HMI but it didn't help. I am not sure if it is possible, but I would save the S7 project first (with reorganization) and recompile (=save) the S7-Graph Block. Than recreate the Proagent data inside the HMI and download everything again. It wouldn't be the first time that something went corrept inside the S7 project data. Hope it will help |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on