5/31/2019 11:11 AM | |
Posts: 6 Rating: (0) |
Hi All, We are planning to communicate S120 CU 230-2PN with normal Microcontroller which has EMAC interface without using any PLC's. Is It possible? |
5/31/2019 9:22 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello ShruGuru; The information in these links could be of interest: - Profinet technology- the easy way to Profinet http://www.profibus.org.pl/index.php?option=com_docman&task=doc_view&gid=182&Itemid=15 - ICSS EMAC LLD developers guide http://wiki.tiprocessors.com/index.php/ICSS_EMAC_LLD_developers_guide The Industrial SDK release from Texas Instruments enables the use of the PRU-ICSS for Ethernet packet processing. This is used to implement several Industrial Ethernet based protocols including Profinet, EtherNet/IP, EtherCAT etc., The SDK contains one example for each protocol. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/01/2019 13:58:50 |
|
Follow us on