9/21/2015 10:52 AM | |
Joined: 10/10/2014 Last visit: 8/28/2024 Posts: 1725 Rating: (210) |
Hi Kiiza Pleas start the tool reset_wincc.vbs and restart your computer. If it dowst help chech follow points 1. Was the computer name altered or does contain special characters? 2. Were carried out the DCOM/Firewall settings with Simatic Security Control? (If yes, please execute it again on the affected station) -> Start-> Simatic-> Simatic Security Control 3. Is the computer in the correct workgroup / domain? 4. Are the authorisations correct? The user must be entered on Simatic HMI and a SQL group, besides, at least power user authorisation (better: Administrator) 5. Are the servers available in the SimaticShell? Recommendation: Right click on SimaticShell -> Update 6. Is the terminal bus in the network configuration at the uppermost place? 7. Please check the following FAQ and particularly the suitable authorisations: http://support.automation.siemens.com/WW/view/en/22559072 8. Is the instance "....\WINCC" selected in the SQL manager and is loaded? 9. Please check the following FAQ: http://support.automation.siemens.com/WW/view/en/26460192 10. Please check the following points in the FAQ 33123686 (http://support.automation.siemens.com/WW/view/en/33123686) 11. Please check the correct target-path of your OS-project (Attend to typing errors!)? 12. Please check the following FAQ, especially the LMHOSTS configuration: http://support.automation.siemens.com/WW/view/de/868014 13. Please check if the simple file sharing is deactivated. (Control Panel, Folder Options, View) 14. Please check if the shared folder has permitted full rights to the user. If this doesn't help please delete the whole OS project from your target station and do a full OS-compile and full OS-download (if possible). Please make sure to save the online data from server. Best regards schufri Normal 0 21 false false false DE X-NONE X-NONE |
This contribution was helpful to4 thankful Users |
7/12/2019 6:03 PM | |
Posts: 1 Rating: (0) |
Hello I used the reset_wincc.vbs tool and reboot your computer and it worked well to correct the error |
8/9/2021 8:48 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello lganson, it is always a good idea, to delete the dcf-files, see FAQ: https://support.industry.siemens.com/cs/ww/en/view/109763043 dcf means "distribuded config file".
|
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on