7/13/2019 10:58 AM | |
Joined: 5/29/2019 Last visit: 6/22/2023 Posts: 12 Rating: (1) |
I appreciate your Answer Sir. But I have one more question If you can elaborate it , I am Using s7-300 With an analog Input which 8Bit . In my analog Input The value corresponding to my 4mA is not Zero in the PLC rather it's 5504. Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/15/2019 07:23:01New subject after splitting Shamoh |
|
7/13/2019 12:20 PM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4148 Rating: (464) |
Post a screen shot of the code you have now (in online), so we can see what you have done now. |
12/10/2019 2:38 PM | |
Posts: 47 Rating: (0) |
Hello OP. There is a formula described in FC105 datasheet. I am attaching it below Page 10/11, in your case, with 4-20mA, the signal is unipolar, therefore k1=0.0, k2=+27648.0.
AttachmentSCALE_FC105.pdf (255 Downloads) |
Follow us on