7/12/2019 7:19 AM | |
Posts: 14 Rating: (1) |
I have some trouble with diagrams in my WinCC project. The diagram in picture "diagram1" is how it should be. When you unselect a parameter, the scale on the right site should disappear too. You can see this in picture "diagram1-settingsChanged". Then I have the diagram2 in my project which does not support this functionality. You can see on the bottom that just two parameters are selected, but on the left side all scales are displayed. I want to change this with a script, but I did not find how to do this. Hopefully, someone know how I can change this. AttachmentDiagram.zip (86 Downloads) |
7/15/2019 2:59 PM | |
Posts: 14 Rating: (1) |
Does it mean that it is not possible to adjust diagrams using scripts? |
7/19/2019 7:28 AM | |
Posts: 14 Rating: (1) |
Thanks for your reply. I solved it with a VBScript. |
Follow us on