5/25/2019 12:08 PM | |
Posts: 2 Rating: (0) |
To résolve this problème i install 'S7-200 PC Access SMART v2.3'. now the problem is resolved and the pg/pc work perfectly. |
7/16/2019 1:54 PM | |
Posts: 1 Rating: (0) |
Hello, For user with Windows 7 in Czech Language. - look to Folder "c:\ProgramData\Siemens\Automation\Simatic OAM\data\LogDevices\" - rename files - you must change Czech chars to English chars. Like on pictures. - then you see your missing Interfaces. If you have not files with your interfeces, you can use ChristophD's solution from 11/24/2014 10:18 AM and then rename file. I hope i helped you Bystricky |
This contribution was helpful to1 thankful Users |
9/19/2019 6:02 AM | |
Joined: 2/13/2019 Last visit: 8/21/2024 Posts: 4 Rating: (0) |
I am also facing same problem but not solved as per above. No access point is showing in pg/pc interface and also no module is showing in add/remove interfaces. I am attaching log file and screenshot for reference. please support i am in a big trouble. Attachments7epaImp64x_2019-09-19 09.16.52.zip (791 Downloads) |
Follow us on