7/18/2019 4:49 PM | |
Joined: 4/4/2019 Last visit: 7/11/2024 Posts: 59 Rating: (2) |
Hi everyone! I have a project in Wincc V7.0 + SP1, and the other I want to take some information about a object and then when I tried to see de Object Propierties I couldnt! None of the project objects. Every time that I tried to see a property from any object the 'blue' of the windows it turns grey like if the windows of Objects Properties it would open but is not. And if I double-clicking an object (normally I use to access the object properties in that way) it opens the graphic properties of Siemens. I look all the properties of the Wincc, I didnt change any of it but anyway I look at and I didnt found anything. Also I reset the Wincc but nothing. I see the same problem but in Wincc Flexible 2008 here https://support.industry.siemens.com/tf/WW/en/posts/object-properties-disabled-wincc-flex-2008/42633?page=0&pageSize=10 But I dont know if this can happen in WinCC v7. Can anyone help me? Thank you very much |
7/18/2019 5:35 PM | |
Joined: 8/5/2008 Last visit: 9/10/2024 Posts: 60 Rating: (11) |
Hello, Often I have fixed many issues by installing the latest update/hotfix for WinCC. Its not so much that the update contains a real fix, but it invokes the installer and acts to repair the installation in some cases. I would suggest this first since you have 7.0Sp1. Also, for a slightly different issue than yours, there is a faq to reset the graphics designer via the Windows registry. It would be worth a try as well. https://support.industry.siemens.com/cs/ww/en/view/70967 Beyond those things, you would be looking at removing all the WinCC software and installing again. In some case if the issue is deeper in Windows, then you'd want to remove the license keys and format Windows which is much quicker to resolve these type issues. Thanks, Steve |
Last edited by: kustomcity at: 07/18/2019 17:35:51 |
|
7/19/2019 8:31 AM | |
Joined: 4/4/2019 Last visit: 7/11/2024 Posts: 59 Rating: (2) |
Wow...I hope not to install again the WinCC again. Thank you anyway, |
Follow us on