7/18/2019 9:30 PM | |
Joined: 1/4/2016 Last visit: 8/12/2024 Posts: 2 Rating: (0) |
is het mogelijk om de firmware van een s7-1200 (es7 212-1BD30-0XB0) v2.2 te updaten naar een v4.2 ? |
8/2/2019 11:04 AM | |
Joined: 5/29/2013 Last visit: 9/20/2024 Posts: 100 Rating: (28) |
Sander, Just like Christoph told, it’s not possible. On this link you will find the download page of the firmware 4.2. Also here it’s mentioned: Compatibility of the hardware and software Existing SIMATIC S7-1200 CPUs V4 (Article No. 6ES721x-1xx40-0XB0) can be updated to the new CPU firmware 4.2. V2.2 is the latest version for your hardware version. |
Last edited by: Jen_Moderator at: 08/02/2019 11:46:01Optimized links. Regards |
|
This contribution was helpful to1 thankful Users |
9/10/2019 4:01 PM | |
Joined: 7/29/2018 Last visit: 3/9/2022 Posts: 2 Rating: (0) |
I think you need to buy a new PLC of firmware V4.2 |
Follow us on