7/19/2019 8:07 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello elaba, the values and timestamps in the Taglogging Archives are stored there in a compressed manner in binary packages. You can read out the values with VB-Scripts, see the Application example: "Export of archive data using the SIMATIC WinCC/Connectivity Pack (OLE DB Provider)" https://support.industry.siemens.com/cs/ww/en/view/38132261 But you can not write data in the Taglogging Archives with such a script. The only way to write data in a Taglogging Archive is, to use the ODK-function "TLGInsertArchivData". This is a C-function. You can display the Taglogging data in a WinCC Table Control, in this WinCC Table Control you have the possibility to edit values manually. Best Regards Georg Berghof AttachmentTLGInsertArchivData.pdf (116 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|
7/22/2019 9:00 AM | |
Posts: 14 Rating: (1) |
Thanks a lot. Really helpful! |
Follow us on